Working with Images on a Handheld

On a handheld, images can be copied from one document to another or resized or repositioned within a document. You can also delete images from a document.

You cannot add or insert images into a document when working on a handheld. However, you can transfer a document containing an image from your computer to a handheld.

Note: If there is not enough storage on the handheld to accommodate a document containing an image, an error message is displayed.

Copying an Image

Complete the following steps to copy an image from one document to another or from one page to another within the same document.

1. Open the document that contains the image you want to copy.
2. Select the image.
• In the Question or Notes applications, move the cursor over the image and press x.
• In the Graphs & Geometry application, press b 1 2 2.
• In the Data & Statistics application, press b 3 6.

A border appears around the image.

3. Press / b, and then click Copy. You can also press / C.
4. Open the document where you want to paste the image or select a page in the current document.

Note: If you open a new document, you will be prompted to save and close the current document.

5. Press / V.

Note: If pasting an image into the Graphs & Geometry application, press ·, and then press / V.

The image is copied to the page in the document.

Repositioning an Image

Complete the following steps to reposition an image on a page.

1. Open the document and navigate to the page that contains the image.
2. Select the image.
• In the Question or Notes applications, move the cursor over the image, and then press, hold, and release x. The image appears shaded.
• In the Graphs & Geometry application, press b 1 2 2.
• In the Data & Statistics application, press b 3 6.

A border appears around the image.

3. Move the image.
• In the Question or Notes applications, move the cursor to the new location and press x.
• In the Graphs & Geometry or Data & Statistics applications:
- Press and hold x until the cursor changes to a four-sided arrow (). The image floats in the background and the border changes to a dashed line.
- Move your finger over the Touchpad to move the image to the new location, and then press x or · to place the image.

Resizing an Image

Complete the following steps to resize an image on a page.

1. Open the document that contains the image.
2. Select the image.
• In the Question or Notes applications, or in Quick Poll, move the cursor over the image and press, hold, and then release x. The image appears shaded.
• In the Graphs & Geometry application, press b 1 2 2.
• In the Data & Statistics application, press b 3 6.

A border appears around the image.

3. Move the cursor to one of the corners.

The cursor changes to a four-sided directional arrow ().

Note: If you move the cursor to the edge of an image, the cursor changes to a two-sided directional arrow. You can drag the image left or right to resize it, but the image will become distorted.

4. Press x.

The tool is enabled.

5. Move your finger over the Touchpad in any direction to resize the image.

A dashed line appears to indicate the new size.

6. To accept the new size, press x or ·.

Deleting an Image

Complete the following steps to remove an image from a page.

1. Open the document that contains the image.
2. Select the image.
• In the Question or Notes applications, move the cursor over the image, and then press, hold, and release x. The image appears shaded.
• In the Graphs & Geometry application, press b 1 2 2.
• In the Data & Statistics application, press b 3 6.

A border appears around the image.

3. Press / b, and then select Delete.

The image is removed.

Note: In the Question and Notes applications, you can also press . to remove a selected image.