OS Upgrade Messages
This section lists the information and error messages that can be displayed on handhelds during an OS Upgrade.
|
Shown on: |
Message and Description |
|
Sending handheld |
“Receiver does not have enough storage space. Make <xxxK> available.“ |
|
This message indicates that the receiving handheld does not have enough storage available for the new OS. The space requirement is shown so you know how much storage must be cleared for the new operating system. Files can be moved to a computer for storage to free the necessary space. |
|
|
Sending handheld |
“Receiver must change batteries before upgrading the OS.“ |
|
This message indicates that the batteries in the receiving handheld need to be replaced. Send the OS Upgrade once the batteries are replaced. |
|
|
Sending handheld |
“Receiver has a newer OS and cannot
OK |
|
This message indicates that the receiving handheld has a newer OS version than the one being transmitted. You cannot downgrade an OS. |
|
|
Sending handheld |
“Upgrade not accepted by receiver.“ OK |
|
This message indicates that the receiving handheld refuses the upgrade. |
|
|
Sending handheld |
“OS has been transferred.
OK |
|
This message indicates that the transfer is complete and it is safe to unplug the cable from the sending handheld. |
|
|
Sending handheld |
“Sending OS. Do not unplug cable.“ |
|
This message, along with a progress bar, is displayed while the OS Upgrade is being transferred. |
|
|
Both handhelds |
“Transfer failed. Check cable and try again.“ OK |
|
The sending and/or receiving handheld is not properly connected. Reinsert the cable into each handheld, and then try the transmission again. |
|
|
Receiving handheld |
“You are receiving an OS Upgrade. Unsaved changes will be lost.
Yes No |
|
This message is displayed when an OS Upgrade is about to begin. If you do not select Yes within 30 seconds, the system automatically responds with No. |
|
|
Receiving handheld |
“Receiving OS. Do not unplug cable.“ |
|
This message, along with a progress bar, is displayed while the OS Upgrade is being transferred. |
|
|
Receiving handheld |
“Installing OS.“ |
|
This message is displayed when the transfer is complete. It is shown to keep you informed of the handheld’s status. |
|
|
Receiving handheld |
“OS has been installed. Handheld will restart.“ OK |
|
This information message displays briefly before the handheld automatically reboots. |
|
|
Receiving handheld |
“Install was corrupted. Handheld will reboot. You will need to retry OS upgrade.“ OK |
|
An error occurred during the transmission and the installation was corrupted. The handheld will reboot. After the reboot, reinstall the OS Upgrade. |