Finding Operating System Updates

For up-to-date information about available OS upgrades, check the Texas Instruments website at education.ti.com.

You can download an OS upgrade from the Texas Instruments website to a computer, and use a USB cable to install the OS on your TI-Nspire™ CX II handheld. You will need an Internet connection and the appropriate USB cable to download the updates.

Checking for Handheld OS Updates

When using TI-Nspire™ software, you can quickly determine if your handheld OS is up to date when the handheld is connected to a computer.

1. Open the TI-Nspire™ software and ensure the handheld is connected to your computer.
2. In the Documents Workspace, click to open Content Explorer.
3. In the Connected Handhelds pane, select a connected handheld.

4. Select Help > Check for Handheld OS Update.
• If the operating system is current, the Check for Handheld OS Update dialog box opens indicating that the operating system on the handheld is up to date.

• If the operating system is not current, the dialog box contains a message indicating that a new version of the operating system is available.
5. Click OK to close the dialog box.