Exploring Content Explorer

Use Content Explorer to:

• See a list of files on your computer.
• Create and manage lesson bundles.
• If using software that supports connected handhelds, you can:
- See a list of files on any connected handheld.
- Update the OS on connected handhelds.
- Transfer files between a computer and connected handhelds.

Note: If you are using TI-Nspire™ software that does not support connected handhelds, the Connected Handheld heading is not shown in the Content Explorer pane.

À

The Documents Toolbox menu.

Á

Shows files on your computer and the name of the folder where the files are located. Click ¤ to navigate to another folder on the computer.

Â

The list of folders and files within the folder named in the Look In: field. Right-click on a highlighted file or folder to open the context menu listing available actions for that file or folder.

Ã

Click to close the list of files. Click to open the list of files.

Ä

Options menu. Click ¤ to open the menu of actions you can perform on a selected file:

• Open an existing file or folder.
• Move (navigate) up one level in the folder hierarchy.
• Create a new folder.
• Create a new lesson bundle.
• Rename a file or folder.
• Copy selected file or folder.
• Paste file or folder copied to Clipboard.
• Delete selected file or folder.
• Select all files in a folder.
• Package lesson bundles.
• Refresh the view.
• Install OS.

Å

Connected handhelds. Lists the connected handhelds. Multiple handhelds are listed if more than one handheld is connected to the computer or when using the TI-Nspire™ Docking Stations.

Æ

The name of the connected handheld. To show the folders and files on a handheld, double-click the name.

Click ¤ to navigate to another folder on the handheld.