Using the Application Menu
The Application menu enables you to select tools for working with a specific application. Each application has a unique menu.
Using the Application Menu
| 1. | From a blank page, press b to display the Application menu. |
The menu displays applications that you can add to the page.
| 2. | Press the number of the application you want to add to the page. For example, press 4 to add the Lists & Spreadsheet application. |
| 3. | Press b to display the Application menu, which lists the options for working with the current application. |
The example below displays the Application menu for the Lists & Spreadsheet application.