Working with Problems and Pages
When you create a new document, it consists of a single problem with a single page. You can insert new problems and add pages to each problem.
A document can contain up to 30 problems. Each problem's variables are unaffected by the variables in other problems.
| ▶ | On the Insert menu, select Problem. —or— Click the Insert tool on the main toolbar, and select Problem. |
A new problem with an empty page is added to your document.
Each problem can contain up to 50 pages. Each page has a work area, where you can perform calculations, create graphs, collect and plot data, or add notes and instructions.
| 1. | Click Insert > Page. —or— Click the Insert tool on the main toolbar, and select Page. |
An empty page is added to the current problem, and you are prompted to choose an application for the page.
| 2. | Select an application to add to the page. |
New problems are named automatically as Problem 1, Problem 2, and so on. To rename a problem:
| 1. | If necessary, click the Page Sorter tool in the Documents Toolbox. |
| 2. | Click the problem name to select it. |
| 3. | On the Edit menu, click Rename. |
| 4. | Type the new name. |
The Page Sorter lets you reorder problems within a document. If you move a problem that you have not renamed, the numeric part of the default name changes to reflect the new position.
| 1. | If necessary, click the Page Sorter tool in the Documents Toolbox. |
| 2. | In the Page Sorter, arrange the problems by dragging each problem name to its new position. |
Tip: To collapse a problem's list of page thumbnails, double-click the name of the problem.
You can copy a problem within the same document or copy it to a different document.
| 1. | If necessary, click the Page Sorter tool in the Documents Toolbox. |
| 2. | Click the problem name to select it. |
| 3. | On the Edit menu, click Copy. |
| 4. | Click the location at which you want to insert the copy. |
| 5. | On the Edit menu, click Paste. |
You can move a problem within the same document or move it to a different document.
| 1. | If necessary, click the Page Sorter tool in the Documents Toolbox. |
| 2. | Click the problem name to select it. |
| 3. | On the Edit menu, click Cut. |
| 4. | Click the new location of the problem. |
| 5. | On the Edit menu, click Paste. |
To delete a problem and its pages from the document:
| 1. | If necessary, click the Page Sorter tool in the Documents Toolbox. |
| 2. | Click the problem name to select it. |
| 3. | On the Edit menu, click Delete. |
Adding a Problem to a Document
on the main toolbar, and select
in the Documents Toolbox.