Formatting Text in Documents

Use the text formatting tools to format text in TI-Nspire™ applications that allow formatted text, and to format text in PublishView™ documents. By default, the text formatting toolbar opens in the area above an active document. Options on the toolbar are enabled or disabled depending on the active application.

Option

Function

Click ¤ to open the menu for the active application. This tool enables you to open an application menu regardless of the option selected in the Documents Toolbox.

Click ¤ to select a background color for highlighting text or choose a fill color for a selected cell.

Click ¤ to select the line color for an object. For example, in Graphs & Geometry, you can choose a color for a selected shape.

Click ¤ to select a color for selected text.

Use these tools to choose a font and set the size of the font.

• Click ¤ to select a different font from the drop-down box.
• To select as specific font size, click ¤ to select a size from the drop-down box.
• Click to increase the font size or click to decrease the font size incrementally.

Click the appropriate tool to apply bolding, italics, or underlining; apply superscript or subscript; or strike out text.

In a PublishView™ document, use these tools to position text within the header or footer, or in text box. Clicking opens the Hyperlink dialog box.

For more information, see Working with PublishView™ Documents.

Hiding and Showing the Formatting Toolbar

▶ When the formatting toolbar is visible, click £ (located under the toolbar) to hide the toolbar.
▶ Click ¤ to show the toolbar when the formatting toolbar is hidden.