Using Motion Match
Use this option to create a randomly generated plot when creating position-versus-time or velocity-versus-time graphs.
This feature is only available when using a motion detector such as the CBR 2™ sensor or the Go!Motion® sensor.
Generating a Motion Match Plot
To generate a plot:
| 1.
|
Attach the motion detector. |
| 4.
|
Select one of the following options: |
| •
|
. Generates a random position plot. |
| •
|
. Generates a random velocity plot. |
Continue selecting a new position or a new velocity match to generate a new random plot without removing the existing plot.
Removing a Motion Match Plot
To remove the generated plot:
| ▶
|
Click Analyze > Motion Match > Remove Match. |