You can replay one data set at a time. By default, the latest data set plays using the first column as the base column (example: time reference).
If you have multiple data sets, and want a different data set or base column than the default, you can select the data set to replay and the base column.
To select the data set to replay:
The Advanced Replay Settings dialog box opens.
| 2.
|
Select the data set to replay from the Data Set drop-down list. |
Note: Changing the run in the Data Set selection tool does not affect the playback choice. You must specify which data set in .
| 3.
|
(Optional) Select a new value from the Base Column drop-down list. |
The selected column acts as the “Time” column for the replay.
Note: The base column should be a strictly increasing list of numbers.
| 4.
|
Click to start the playback and save the settings. |
Note: Data Set and Base Column options are based on the number of stored runs and the sensor type used.