Recharging the Handheld

To recharge the TI-Nspire™ Rechargeable Battery in a handheld, connect it to any of the following power sources:

• A standard USB cable connected to a computer
• A TI USB wall charger (sold separately)
• A TI-Nspire™ CX Docking Station if in a classroom setting

The amount of time required to fully charge the battery may vary, but charging normally takes about six hours. It is not necessary to remove the TI-Nspire™ Rechargeable Battery from the handheld to recharge it. The handheld operates normally while it is attached to a charging source.

Recharging a Battery from a Computer

To recharge a handheld from a computer, a TI-Nspire™ USB driver must be installed. USB drivers are standard with any TI-Nspire™ software, which includes:

• TI-Nspire™ CX Premium Teacher Software
• TI-Nspire™ CX CAS Premium Teacher Software
• TI-Nspire™ CX Student Software
• TI-Nspire™ CX CAS Student Software

To download software that includes a driver, go to education.ti.com/software.

Understanding the Priority of Power Sources

When the TI-Nspire™ Rechargeable Battery is fully charged, the handheld draws power in the following order:

• First, from a connected external power source, such as:
- A computer connected through a standard USB cable
- An approved wall charger (sold separately)
• Second, from the TI-Nspire™ Rechargeable Battery

Disposing of Used Batteries Safely and Properly

Do not mutilate, puncture or dispose of batteries in fire. The batteries can burst or explode, releasing hazardous chemicals. Discard used batteries according to local regulations.