Exploring the Class Record
From the Class Record, you can open a document in the Review Workspace; save a document to the Portfolio Workspace; collect files from the Class Record Workspace; send and delete files using the toolbar; and view document properties in Record Item Properties for all TI-Nspire™ documents, except Quick Poll files.
By default, 100 records are listed. To see additional records, click Load Next 100 or click Load All Entries.
À |
File action. The icons indicate the status of a file. Sent to class Collected from class Saved to portfolio Redistributed to class Quick Poll Unprompted Deleted |
Á |
File name. The names of files used in this class. |
 |
Status. The progress of an action. For example, "23 of 25" indicates that 23 out of 25 students have received a file. |
à |
Menu options. Click ¢ for quick access to certain menu items. This icon gives you the same options as a right-click. |