Setting View Options in Capture Class

You have several options for optimizing the view of captured class screens, including:

• Toggling between a tiled view and a gallery view.
• Comparing selected screens in a side-by-side view.
• Refreshing the view as needed or setting the auto-refresh feature to automatically refresh the view at timed intervals.
• Zooming in or out to increase or decrease the size of the captured screens in the window. You can also select the percentage at which the size of the screen will be increased or decreased.
• Showing or hiding student names.
• Accessing Live Presenter options. For more information, see Using Live Presenter.