Using Sensor Data in Programs
You can access sensor data from all connected sensor probes through your TI-Basic program by using this command:
RefreshProbeVars statusVar
• | You must first launch the Vernier DataQuest™ application, or you will receive an error. ![]() |
Note: The Vernier DataQuest™ application will auto-launch when you connect a sensor or a lab cradle to the TI-Nspire™ software or handheld.
• | The RefreshProbeVars command will be valid only when Vernier DataQuest™ is in 'meter' mode.![]() |
• | statusVar is an optional parameter that indicates the status of the command. These are the statusVar values: |
StatusVar Value |
Status |
---|---|
statusVar=0 |
Normal (continue with the program) |
statusVar=1 |
The Vernier DataQuest™ application is in data collection mode. Note: The Vernier DataQuest™ application must be in meter mode for this command to work. |
statusVar=2 |
The Vernier DataQuest™ application is not launched. |
statusVar=3 |
The Vernier DataQuest™ application is launched, but you have not connected any probes. Note: The |
• | Your TI-Basic program will read directly from Vernier DataQuest™ variables in the symbol table. |
• | The meter.time variable shows the last value of the variable; it does not update automatically. If no data collection has occurred, meter.time will be 0 (zero). |
• | Use of variable names without corresponding probes being physically attached will result in a "Variable not defined" error. |
• | The RefreshProbeVars command will be a NOP (null command) on iOS. |
Collecting Sensor Data using RefreshProbeVars
1. | Launch the Vernier DataQuest™ application. |
2. | Connect the sensor(s) you need to collect the data. |
3. | Run the program you wish to use to collect data in the calculator application. |
4. | Manipulate the sensors and collect the data. |
Note: You may create a program to interact with the TI-Innovator Hub using b> Hub > Send. (See Example 2, below.) This is optional.
Example 1
Define temp()=
Prgm
© Check if system is ready
RefreshProbeVars status
If status=0 Then
Disp "ready"
For n,1,50
RefreshProbeVars status
temperature:=meter.temperature
Disp "Temperature: ",temperature
If temperature>30 Then
Disp "Too hot"
EndIf
© Wait for 1 second between samples
Wait 1
EndFor
Else
Disp "Not ready. Try again later"
EndIf
EndPrgm
Example 2- with TI-Innovator™ Hub
Define tempwithhub()=
Prgm
© Check if system is ready
RefreshProbeVars status
If status=0 Then
Disp "ready"
For n,1,50
RefreshProbeVars status
temperature:=meter.temperature
Disp "Temperature: ",temperature
If temperature>30 Then
Disp "Too hot"
© Play a tone on the Hub
Send "SET SOUND 440 TIME 2"
EndIf
© Wait for 1 second between samples
Wait 1
EndFor
Else
Disp "Not ready. Try again later"
EndIf
EndPrgm