Graphing from Notes and Calculator
You can graph a function or relation directly from its context menu. This feature is available for many functions and relations on Notes and Calculator pages.
|
|
If page layout options allow, the graph appears on the same page as the function or relation. Otherwise, the graph appears on a separate Graphs page.
The type of graph created depends on the type of function or relation.
Example of Graphing from Notes
This example uses a Notes page to explore a quadratic function interactively.
| 1. | Insert a math box on a new Notes page, and enter the following function definition: |
Define f1(x)=x2-1·x-4
| 2. | Tap the expression to display its context menu. |
| 3. | Select Graph. |
The graph appears. The graph and the math box are linked so that any adjustment to one affects the other.
| 4. | Explore the relationship between the defined function and its graph: |
| - | Drag the ends or center of the graph to manipulate it, and observe the changes to the function definition. |
—or—
| - | Edit the defined function in the math box, and observe the changes to the graph. |