Graphing a Scatter Plot

1. In the Graphs application, tap Tools  and go to Graph Entry/Edit > Scatter Plot.

2. Use one of the following methods to specify two lists to plot as x and y.
- Tap to select a list variable that you have defined in the current problem.
- Type the name of an existing list variable, such as v1.
- Type the list elements directly (for example, type {1,2,3}.

3. Tap ENTER to plot the data, and then zoom the work area to view the plotted data.