Accessing the Graph History

For each problem, the Graphs application automatically stores a history of defined relations, such as functions f1 through f99 and sequences u1 through u99. You can view and edit these items.

Viewing the History of the Current Relation Type

1. Tap History  at the right end of the Graphs toolbar to show the history of the current relation type (for example, f for Functions).

2. In the History list, tap the name of the relation, and then tap Done to show the relation in the entry line.
3. Use the up and down arrow keys to scroll through the defined relations.

Viewing the History of other Relation Types

1. In the Graphing view, tap Tools , go to Graph Entry/Edit, and tap the relation type. For example, tap Polar to show an entry line for the next available Polar relation.
2. Use the up and down arrow keys to scroll through the defined relations.