Changing Document Settings
Document settings control how all numbers, including elements or matrices and lists, are displayed in TI-Nspire™ documents. You can change the default settings at any time, and you can specify settings for a specific document.
Complete the following steps to customize the settings that are applied to your document.
|
1.
|
Create a new document or open an existing document. |
|
2.
|
Tap . |
When you open Document Settings the first time, the default settings are displayed.
|
3.
|
Tap the menu name to open the menu and view the available values for each setting. |
|
Display Digits
|
|
|
Angle
|
|
|
Exponential Format
|
|
|
Real or Complex Format
|
|
|
Calculation Mode
|
Note: Auto mode shows an answer that is not a whole number as a fraction except when a decimal is used in the problem. Exact mode (CAS) shows an answer that is not a whole number as a fraction or in symbolic form, except when a decimal is used in the problem.
|
|
CAS Mode
|
Note: This option is only available on CAS handhelds and software.
|
|
Vector Format
|
|
|
Base
|
|
|
Unit System (CAS)
|
Note: This option is only available on CAS handhelds and software.
|
|
4.
|
Select the desired settings. |
|
5.
|
Choose one of the following options: |
|
•
|
To apply the customized settings to ALL documents, tap . |
|
•
|
To apply the settings to the open document only, tap . |
|
•
|
To restore default settings, tap . |