Entering Simple Math Expressions
Note: To enter a negative number, tap
instead of the minus sign.
Suppose you want to evaluate
.
| 1. | Tap an entry line in the Calculator work area. |
| 2. | Tap to begin the expression. |
| 3. | Tap to return the cursor to the baseline. |
| 4. | To complete the expression: |
Tap
.
| 5. | Tap ENTER to evaluate the expression. |
The expression is displayed in standard mathematical notation, and result is displayed on the right side of the entry line. If a result does not fit on the same line with the expression, it is displayed on the next line.
The expression and the result are added to the Calculator history.
to begin the expression.
to return the cursor to the baseline.