G
Catalog > |
|
gcd(Number1, Number2) ⇒ expression Returns the greatest common divisor of the two arguments. The gcd of two fractions is the gcd of their numerators divided by the lcm of their denominators. In Auto or Approximate mode, the gcd of fractional floating-point numbers is 1.0. |
|
gcd(List1, List2) ⇒ list Returns the greatest common divisors of the corresponding elements in List1 and List2. |
|
gcd(Matrix1, Matrix2) ⇒ matrix Returns the greatest common divisors of the corresponding elements in Matrix1 and Matrix2. |
|
Catalog > |
|
geomCdf(p,lowBound,upBound) ⇒ number if lowBound and upBound are numbers, list if lowBound and upBound are lists geomCdf(p,upBound)for P(1≤X≤upBound) ⇒ number if upBound is a number, list if upBound is a list Computes a cumulative geometric probability from lowBound to upBound with the specified probability of success p. For P(X ≤ upBound), set lowBound = 1. |
|
Catalog > |
|
geomPdf(p,XVal) ⇒ number if XVal is a number, list if XVal is a list Computes a probability at XVal, the number of the trial on which the first success occurs, for the discrete geometric distribution with the specified probability of success p. |
|
Hub Menu |
|||||||
Programming command: Retrieves a value from a connected TI-Innovator™ Hub and assigns the value to variable var. The value must be requested:
— or —
Implicit simplification takes place. For example, a received string of "123" is interpreted as a numeric value. To preserve the string, use GetStr instead of Get. |
Example: Request the current value of the hub's built-in light-level sensor. Use Get to retrieve the value and assign it to variable lightval.
Embed the READ request within the Get command.
|
||||||
If you include the optional argument statusVar, it is assigned a value based on the success of the operation. A value of zero means that no data was received. |
|
||||||
In the second syntax, the func() argument allows a program to store the received string as a function definition. This syntax operates as if the program executed the command: Define func(arg1, ...argn) = received string The program can then use the defined function func(). Note: You can use the Get command within a user-defined program but not within a function. |
Catalog > |
|
getDenom(Expr1) ⇒ expression Transforms the argument into an expression having a reduced common denominator, and then returns its denominator. |
|
Catalog > |
|||||||
getKey([0|1]) ⇒ returnString Description:getKey() - allows a TI-Basic program to get keyboard input - handheld, desktop and emulator on desktop. Example:
|
Example:
|
Handling of key presses:
Handheld Device/Emulator Key |
Desktop |
Return Value |
---|---|---|
Esc |
Esc |
"esc" |
Touchpad - Top click |
n/a |
"up" |
On |
n/a |
"home" |
|
|
|
Scratchapps |
n/a |
"scratchpad" |
Touchpad - Left click |
n/a |
"left" |
Touchpad - Center click |
n/a |
"center" |
Touchpad - Right click |
n/a |
"right" |
Doc |
n/a |
"doc" |
|
|
|
Tab |
Tab |
"tab" |
Touchpad - Bottom click |
Down Arrow |
"down" |
Menu |
n/a |
"menu" |
|
|
|
Ctrl |
Ctrl |
no return |
Shift |
Shift |
no return |
Var |
n/a |
"var" |
Del |
n/a |
"del" |
|
|
|
= |
= |
"=" |
trig |
n/a |
"trig" |
0 through 9 |
0-9 |
"0" ... "9" |
Templates |
n/a |
"template" |
Catalog |
n/a |
"cat" |
|
|
|
^ |
^ |
"^" |
X^2 |
n/a |
"square" |
/ (division key) |
/ |
"/" |
* (multiply key) |
* |
"*" |
e^x |
n/a |
"exp" |
10^x |
n/a |
"10power" |
+ |
+ |
"+" |
- |
- |
"-" |
|
|
|
( |
( |
"(" |
) |
) |
")" |
. |
. |
"." |
(-) |
n/a |
"-" (negate sign) |
Enter |
Enter |
"enter" |
|
|
|
ee |
n/a |
"E" (scientific notation E) |
a - z |
a-z |
alpha = letter pressed (lower case) ("a" - "z") |
shift a-z |
shift a-z |
alpha = letter pressed "A" - "Z" |
|
|
Note: ctrl-shift works to lock caps |
?! |
n/a |
"?!" |
|
|
|
pi |
n/a |
"pi" |
Flag |
n/a |
no return |
|
|
|
, |
, |
"," |
Return |
n/a |
"return" |
Space |
Space |
" " (space) |
|
|
|
Inaccessible |
Special Character Keys like @,!,^, etc. |
The character is returned |
n/a |
Function Keys |
No returned character |
n/a |
Special desktop control keys |
No returned character |
Inaccessible |
Other desktop keys that are not available on the calculator while getkey() is waiting for a keystroke. ({, },;, :, ...) |
Same character you get in Notes (not in a math box) |
Note: It is important to note that the presence of getKey() in a program changes how certain events are handled by the system. Some of these are described below.
Terminate program and Handle event - Exactly as if the user were to break out of program by pressing the ON key
"Support" below means - System works as expected - program continues to run.
Event |
Device |
Desktop - TI-Nspire™ Student Software |
---|---|---|
Quick Poll |
Terminate program, handle event |
Same as the handheld ( |
Remote file mgmt
(Incl. sending 'Exit Press 2 Test' file from another handheld or desktop-handheld) |
Terminate program, handle event |
Same as the handheld. ( |
End Class |
Terminate program, handle event |
Support ( |
Event |
Device |
Desktop - TI-Nspire™ All Versions |
|
Support - Can successfully issue commands to the |
Same as the handheld |
Catalog > |
|
getLangInfo() ⇒ string Returns a string that corresponds to the short name of the currently active language. You can, for example, use it in a program or function to determine the current language. English = “en” |
|
Catalog > |
|
Returns the current locked/unlocked state of variable Var. value =0: Var is unlocked or does not exist. value =1: Var is locked and cannot be modified or deleted. |
|
Catalog > |
|
getMode(ModeNameInteger) ⇒ value getMode(0) ⇒ list getMode(ModeNameInteger) returns a value representing the current setting of the ModeNameInteger mode. getMode(0) returns a list containing number pairs. Each pair consists of a mode integer and a setting integer. For a listing of the modes and their settings, refer to the table below. If you save the settings with getMode(0) → var, you can use setMode(var) in a function or program to temporarily restore the settings within the execution of the function or program only. See setMode(), here. |
|
Mode |
Mode |
|
Display Digits |
1 |
1=Float, 2=Float1, 3=Float2, 4=Float3, 5=Float4, 6=Float5, 7=Float6, 8=Float7, 9=Float8, 10=Float9, 11=Float10, 12=Float11, 13=Float12, 14=Fix0, 15=Fix1, 16=Fix2, 17=Fix3, 18=Fix4, 19=Fix5, 20=Fix6, 21=Fix7, 22=Fix8, 23=Fix9, 24=Fix10, 25=Fix11, 26=Fix12 |
Angle |
2 |
1=Radian, 2=Degree, 3=Gradian |
Exponential Format |
3 |
1=Normal, 2=Scientific, 3=Engineering |
Real or Complex |
4 |
1=Real, 2=Rectangular, 3=Polar |
Auto or Approx. |
5 |
1=Auto, 2=Approximate |
Vector Format |
6 |
1=Rectangular, 2=Cylindrical, 3=Spherical |
Base |
7 |
1=Decimal, 2=Hex, 3=Binary |
Unit system |
8 |
1=SI, 2=Eng/US |
Catalog > |
|
getNum(Expr1) ⇒ expression Transforms the argument into an expression having a reduced common denominator, and then returns its numerator. |
|
Hub Menu |
|
Programming command: Operates identically to the Get command, except that the retrieved value is always interpreted as a string. By contrast, the Get command interprets the response as an expression unless it is enclosed in quotation marks (""). |
For examples, see Get. |
Catalog > |
|
Returns a string that indicates the data type of variable var. If var has not been defined, returns the string "NONE". |
|
Catalog > |
|
getVarInfo() ⇒ matrix or string getVarInfo(LibNameString) ⇒ matrix or string getVarInfo() returns a matrix of information (variable name, type, library accessibility, and locked/unlocked state) for all variables and library objects defined in the current problem. If no variables are defined, getVarInfo() returns the string "NONE". getVarInfo(LibNameString)returns a matrix of information for all library objects defined in library LibNameString. LibNameString must be a string (text enclosed in quotation marks) or a string variable. If the library LibNameString does not exist, an error occurs. |
|
Note the example, in which the result of getVarInfo() is assigned to variable vs. Attempting to display row 2 or row 3 of vs returns an “Invalid list or matrix” error because at least one of elements in those rows (variable b, for example) revaluates to a matrix. This error could also occur when using Ans to reevaluate a getVarInfo() result. The system gives the above error because the current version of the software does not support a generalized matrix structure where an element of a matrix can be either a matrix or a list. |
|
Catalog > |
|
Goto labelName Transfers control to the label labelName. labelName must be defined in the same function using a Lbl instruction. Note for entering the example: For instructions on entering multi-line program and function definitions, refer to the Calculator section of your product guidebook. |
|
Catalog > |
|
Expr1►Grad ⇒ expression Converts Expr1 to gradian angle measure. Note: You can insert this operator from the computer keyboard by typing @>Grad. |
In Degree angle mode:
|