D
Catalog > |
|
dbd(date1,date2) ⇒ value Returns the number of days between date1 and date2 using the actual-day-count method. date1 and date2 can be numbers or lists of numbers within the range of the dates on the standard calendar. If both date1 and date2 are lists, they must be the same length. date1 and date2 must be between the years 1950 through 2049. You can enter the dates in either of two formats. The decimal placement differentiates between the date formats. MM.DDYY (format used commonly in the United States) |
|
Catalog > |
|
Expr1 ►DD ⇒ valueList1 Note: You can insert this operator from the computer keyboard by typing @>DD. Returns the decimal equivalent of the argument expressed in degrees. The argument is a number, list, or matrix that is interpreted by the Angle mode setting in gradians, radians or degrees. |
In Degree angle mode:
|
Catalog > |
|
List1 ►Decimal ⇒ expression Matrix1 ►Decimal ⇒ expression Note: You can insert this operator from the computer keyboard by typing @>Decimal. Displays the argument in decimal form. This operator can be used only at the end of the entry line. |
|
Catalog > |
|
Define Var = Expression Defines the variable Var or the user-defined function Function. Parameters, such as Param1, provide placeholders for passing arguments to the function. When calling a user-defined function, you must supply arguments (for example, values or variables) that correspond to the parameters. When called, the function evaluates Expression using the supplied arguments. Var and Function cannot be the name of a system variable or built-in function or command. Note: This form of Define is equivalent to executing the expression: expression → Function(Param1,Param2). |
|
Define Function(Param1, Param2, ...) = Func
Define Program(Param1, Param2, ...) = Prgm In this form, the user-defined function or program can execute a block of multiple statements. Block can be either a single statement or a series of statements on separate lines. Block also can include expressions and instructions (such as If, Then, Else, and For). Note for entering the example: For instructions on entering multi-line program and function definitions, refer to the Calculator section of your product guidebook. Note: See also Define LibPriv, here, and Define LibPub, here. |
|
Catalog > |
|
Define LibPriv Var = Expression Define LibPriv Function(Param1, Param2, ...) = Func Define LibPriv Program(Param1, Param2, ...) = Prgm Operates the same as Define, except defines a private library variable, function, or program. Private functions and programs do not appear in the Catalog. |
|
Catalog > |
|
Define LibPub Var = Expression Define LibPub Function(Param1, Param2, ...) = Func Define LibPub Program(Param1, Param2, ...) = Prgm Operates the same as Define, except defines a public library variable, function, or program. Public functions and programs appear in the Catalog after the library has been saved and refreshed. |
|
See ΔList(), here. |
|
|
|
See ΔtmpCnv(), here. |
|
|
|
Catalog > |
|
DelVar Var1[, Var2] [, Var3] ... DelVar Var. Deletes the specified variable or variable group from memory. If one or more of the variables are locked, this command displays an error message and deletes only the unlocked variables. See |
|
DelVar Var. deletes all members of the Var. variable group (such as the statistics stat.nn results or variables created using the LibShortcut() function). The dot (.) in this form of the DelVar command limits it to deleting a variable group; the simple variable Var is not affected. |
|
Catalog > |
|
Returns a list that has the contents of List1 with all empty (void) elements removed. For more information on empty elements, see here. |
|
See d(), here. |
|
|
|
Catalog > |
|||||||
det(squareMatrix[, Tolerance]) ⇒ expression Returns the determinant of squareMatrix. Optionally, any matrix element is treated as zero if its absolute value is less than Tolerance. This tolerance is used only if the matrix has floating-point entries and does not contain any symbolic variables that have not been assigned a value. Otherwise, Tolerance is ignored.
|
|
Catalog > |
|
diag(List) ⇒ matrix Returns a matrix with the values in the argument list or matrix in its main diagonal. |
|
diag(squareMatrix) ⇒ rowMatrix Returns a row matrix containing the elements from the main diagonal of squareMatrix. squareMatrix must be square. |
|
Catalog > |
|
dim(List) ⇒ integer Returns the dimension of List. |
|
dim(Matrix) ⇒ list Returns the dimensions of matrix as a two-element list {rows, columns}. |
|
dim(String) ⇒ integer Returns the number of characters contained in character string String. |
|
Catalog > |
|
Disp exprOrString1 [, exprOrString2] ... Displays the arguments in the Calculator history. The arguments are displayed in succession, with thin spaces as separators. Useful mainly in programs and functions to ensure the display of intermediate calculations. Note for entering the example: For instructions on entering multi-line program and function definitions, refer to the Calculator section of your product guidebook. |
|
Catalog > |
|||||
DispAt int,expr1 [,expr2 ...] ... DispAt allows you to specify the line where the specified expression or string will be displayed on the screen. The line number can be specified as an expression. Please note that the line number is not for the entire screen but for the area immediately following the command/program. This command allows dashboard-like output from programs where the value of an expression or from a sensor reading is updated on the same line. DispAt and Disp can be used within the same program. Note: The maximum number is set to 8 since that matches a screen-full of lines on the handheld screen - as long as the lines don't have 2D math expressions. The exact number of lines depends on the content of the displayed information.
|
Example
Illustrative examples:
|
Error conditions:
Error Message |
Description |
---|---|
DispAt line number must be between 1 and 8 |
Expression evaluates the line number outside the range 1-8 (inclusive) |
Too few arguments |
The function or command is missing one or more arguments. |
No arguments |
Same as current 'syntax error' dialog |
Too many arguments |
Limit argument. Same error as Disp. |
Invalid data type |
First argument must be a number. |
Void: DispAt void |
"Hello World" Datatype error is thrown for the void (if the callback is defined) |
Conversion operator: DispAt 2_ft @> _m, "Hello World" |
CAS: Datatype Error is thrown (if the callback is defined) Numeric: Conversion will be evaluated and if the result is a valid argument, DispAt print the string at the result line. |
Catalog > |
|
List ►DMS Matrix ►DMS Note: You can insert this operator from the computer keyboard by typing @>DMS. Interprets the argument as an angle and displays the equivalent DMS (DDDDDD°MM'SS.ss'') number. See °, ', '' on here for DMS (degree, minutes, seconds) format. Note: ►DMS will convert from radians to degrees when used in radian mode. If the input is followed by a degree symbol ° , no conversion will occur. You can use ►DMS only at the end of an entry line. |
In Degree angle mode:
|
Catalog > |
|
domain(Expr1, Var) ⇒expression Returns the domain of Expr1 with respect to Var. domain() can be used to examine domains of functions. It is restricted to real and finite domain. This functionality has limitations due to shortcomings of computer algebra simplification and solver algorithms. Certain functions cannot be used as arguments for domain(), regardless of whether they appear explicitly or within user-defined variables and functions. In the following example, the expression cannot be simplified because ∫() is a disallowed function.
|
|
Catalog > |
|
dominantTerm(Expr1, Var [, Point]) ⇒ expression dominantTerm(Expr1, Var [, Point]) | Var>Point ⇒ expression dominantTerm(Expr1, Var [, Point]) | Var<Point ⇒ expression Returns the dominant term of a power series representation of Expr1 expanded about Point. The dominant term is the one whose magnitude grows most rapidly near Var = Point. The resulting power of (Var − Point) can have a negative and/or fractional exponent. The coefficient of this power can include logarithms of (Var − Point) and other functions of Var that are dominated by all powers of (Var − Point) having the same exponent sign. Point defaults to 0. Point can be ∞ or −∞, in which cases the dominant term will be the term having the largest exponent of Var rather than the smallest exponent of Var. dominantTerm(…) returns “dominantTerm(…)” if it is unable to determine such a representation, such as for essential singularities such as sin(1/z) at z=0, e−1/z at z=0, or ez at z = ∞ or −∞. If the series or one of its derivatives has a jump discontinuity at Point, the result is likely to contain sub-expressions of the form sign(…) or abs(…) for a real expansion variable or (-1)floor(…angle(…)…) for a complex expansion variable, which is one ending with “_”. If you intend to use the dominant term only for values on one side of Point, then append to dominantTerm(...) the appropriate one of “| Var > Point”, “| Var < Point”, “| “Var ≥ Point”, or “Var ≤ Point” to obtain a simpler result. dominantTerm() distributes over 1st-argument lists and matrices. dominantTerm() is useful when you want to know the simplest possible expression that is asymptotic to another expression as Var→Point. dominantTerm() is also useful when it isn’t obvious what the degree of the first non-zero term of a series will be, and you don’t want to iteratively guess either interactively or by a program loop. Note: See also series(), here. |
|
Catalog > |
|
dotP(List1, List2) ⇒ expression Returns the “dot” product of two lists. |
|
dotP(Vector1, Vector2) ⇒ expression Returns the “dot” product of two vectors. Both must be row vectors, or both must be column vectors. |
|
See Also: TI-Nspire™ CX II - Draw Commands