19.9.24 setElasticIterations

self = physics.Space:setElasticIterations(iters)

Parameter

Type

Description

self

in physics.Space

The input simulation Space

iters

in number

The number of iterations to use in the impulse solver to solve elastic collisions. Defaults to 0

self

out physics.Space

The input Space is returned as the output

Introduced in platform.apiLevel = '2.0'