19.5.17
setSensor
elf = physics.Shape:setSensor(bool)
Parameter |
Type |
Description |
---|---|---|
self |
in physics.Shape |
The input Shape |
bool |
in boolean |
True if the shape is a sensor |
self |
out physics.Shape |
The input Shape is returned as the output |
Determines if the shape is a sensor (true) or not (false). Sensors call collision handlers but do not generate collisions. Returns self.
Introduced in platform.apiLevel = '2.0'