19.5.11
setCollisionType
self = physics.Shape:setCollisionType(collisionType)
Parameter |
Type |
Description |
---|---|---|
self |
in physics.Shape |
The input Shape |
collisionType |
in number |
Programmer-defined type of collision |
self |
out physics.Shape |
The input Shape is returned as the output |
Assigns a collision type (an integer value of your choosing) to the shape. It is used to determine which handler to call when a collision occurs. Returns self.
Introduced in platform.apiLevel = '2.0'