19.4.29 setVLimit

self = physics.Body:setVLimit(limit)

Parameter

Type

Description

self

in physics.Body

The input Body

limit

in number

The maximum speed of the Body

self

out physics.Body

The input Body is returned as the output

Sets the limit for the maximum speed of the body.

Returns the Body.

Introduced in platform.apiLevel = '2.0'