19.4.23 setMoment

self = physics.Body:setMoment(moment)

Parameter

Type

Description

self

in physics.Body

The input Body

moment

in number

The moment of inertia of the Body

self

out physics.Body

The input Body is returned as the output


Updates the moment of inertia of the body.

Use the provided helper functions to compute the moment of inertia.

Returns the Body.

.Introduced in platform.apiLevel = '2.0'