You can enter and use several types of data, including real and complex numbers, matrices, lists, functions, stat plots, graph databases, graph pictures, and strings.
The TI-84 Plus CE Python uses assigned names for variables and other items saved in memory. For lists, you also can create your own five-character names.
Variable Type |
Names |
Real numbers (including fractions) |
A, B, ... , Z, q |
Complex numbers |
A, B, ... , Z, q |
Matrices |
ãAä, ãBä, ãCä, ... , ãJä To enter a matrix name: Press y ¾. The Matrix Names menu appears. Press the number on the keypad that corresponds with the desired Matrix Name.
|
Lists* |
L1, L2, L3, L4, L5, L6, and user-defined names |
Functions |
Y1, Y2, ... , Y9, Y0 |
Parametric equations |
X1T and Y1T, ... , X6T and Y6T |
Polar functions |
r1, r2, r3, r4, r5, r6 |
Sequence functions |
u, v, w |
Stat plots |
Plot1, Plot2, Plot3 |
Graphical databases |
GDB1, GDB2, ... , GDB9, GDB0 Save current equations from Y= and Window settings to re-use. |
Background images |
Image1, Image2, ... , Image9, Image0 |
Pictures |
Pic1, Pic2, ... , Pic9, Pic0 |
Strings |
Str1, Str2, ... , Str9, Str0 |
Apps |
Applications |
AppVars |
Application variables |
Groups |
Grouped variables Save a group of allowed calculator files for sharing or to re-use when setting up a classroom. |
System variables |
Xmin, Xmax, and others |
* Once a list contains a complex number, it is designated as a complex list. To change a list to Real numbers, delete the list and enter the Real values.
• | You can create as many list names as memory will allow. |
• | From the home screen or from a program, you can store to matrices, lists, strings, and system variables such as Xmax, TblStart, and all Y= functions. |
• | From an editor, you can store to matrices, lists, and Y= functions. |
• | From the home screen, a program, or an editor, you can store a value to a matrix element or a list element. |
• | You can use DRAW STO menu items to store and recall Pic Vars. |
• | Although most variables can be archived, system variables including r, T, X, Y, and q cannot be archived. |
Note: In TI-Basic programming, it is best practice to avoid using these system variables to avoid unexpected changes in the variable value due to calculations and graphing when executing a program.
• | Apps are independent applications, which are stored in Flash archive. AppVars is a variable holder used to store variables created by independent applications. You cannot edit or change variables in AppVars unless you do so through the application that created them. |