Using the Special Character Set

After you select your desired language, a new item (CHARACTER) is added to the
TI-84 Plus CE Python CATALOG. This item accesses special characters and accent marks used in the language that you chose for localization. You can use these special characters and accent marks for display messages and text strings that you want to store to a variable. You cannot, however, use them in variable names.

1. Press y N to display the CATALOG.

Note: CHARACTER is always the first item in the CATALOG.

2. Press [enter] to display the CHARACTER screen.

Accent marks appear in the menus at the bottom of the screen.

3. You can:
Select a special character:
a) Press |, ~, , or } to move the box to the special character that you want to use in a message or text string.
b) Press [enter] to place the character on the edit line.
c) Press |, ~, , or } to move the box to Done.
d) Press [enter] to paste the contents of the edit line to the previous screen.

-or-

 

Add an accent mark to a character:
a) Press the function key (^, _, `, a, or b) immediately above the accent mark to select it. The ALPHA uppercase mode is automatically turned on. To change to lowercase, press ƒ.
b) Press the key associated with the alpha character that you want to accent, for example, [A] (above »). The accented character is displayed in the edit line.
c) Press |, ~, , or } to move the box to Done.
d) Press [enter] to paste the contents of the edit line to the previous screen.