Selecting an Item from a Menu

You can select an item from a menu in three ways.

Press the number or letter of the item you want to select. The cursor can be anywhere on the menu, and the item you select does not need to be displayed on the screen.

-or-

 

Press or } to move the cursor to the item you want, and then press [enter].

-or-

 

Within the Catalog listing of functionality, move the cursor to the item you want, and then press Ã. For most commands, the Catalog Help syntax editor displays the correct syntax. Enter the syntax using the displayed help, and then press ƒ a to paste. The Catalog Help pastes the complete command.
Press ƒ b to escape without pasting the command.

Notes:

After you select an item from a menu, the calculator typically displays the previous screen.
If you do not see PASTE on the Catalog Help screen, press y 5 until you return to the home screen, then repeat your actions. If this happens, it may mean the screens were layered and the previous screen did not have an active cursor on an input line to accept the pasting of the function or command.