You can re-enable all disabled calculator files by using one of the following methods:
• | Link two TI-84 Plus CE Python graphing calculators using a unit-to-unit USB cable and then transfer a file by using y 8, SEND RECEIVE. |
• | Use TI Connect™ CE Actions > Quit Exam Mode on Connected CE Calculators to quit the exam mode on any connected CE calculator. You may also send a calculator file to the connected CE calculator to quit from exam mode. |
• | Use TI Connect™ CE to send a calculator file to the calculator. |
To clear a calculator of files created during an exam:
1. | Turn off the calculator while in test mode. |
2. | "Re-Press-to-Test" - press and hold down the ~, |, and É keys, and then release. |
3. | Select OK when you see the Reset Verification Screen. The calculator is now "clean." |
Tip: To preserve battery life, take your calculator out of Press-to-Test mode after the exam. |