When the TI-84 Plus CE Python detects an error, it returns an error message with a short description.
1:Quit |
Displays the home screen |
2:Goto |
Displays the previous screen with the cursor at or near the error location |
Note: If a syntax error occurs in the contents of a Y= function during program execution, then the 2:Goto option returns to the Y= editor, not to the program.