You should make sure the TI-84 Plus CE Python battery is charged for classroom use and before exams.
Use one of the following options to charge the battery in the TI-84 Plus CE Python graphing calculator:
| • | Connect the graphing calculator to a computer using a USB computer cable. |
-or-
| • | Connect to a wall outlet using a TI wall adapter (may be sold separately). |
-or-
| • | Place the graphing calculator in a TI Charging Station CE. |
The amount of time required to fully charge the battery may vary, but charging takes approximately four hours. It is not necessary to remove the TI Rechargeable Battery from the graphing calculator to recharge it. The graphing calculator operates normally while it is attached to a charging source.
To recharge a graphing calculator from a computer, a TI USB driver must be installed. To download TI Connect™ CE or TI-SmartView™ CE software that includes a driver, go to: education.ti.com/go/download.