Preparing Charging Stations for Use

The TI Charging Station CE is shipped with the following components in each package:

• A TI Charging Station CE
• An AC adapter
• A regional power cord adapter
1. Insert the small end of the power adapter cord into the charging station’s power jack.
2. Plug the other end of the adapter into a power outlet.
• An indentation on each side of the TI Charging Station CE enables you to lift it. Always use two hands to lift and move the charging station.
• Place the charging station on a flat, stable surface. You can also use a wheeled cart if you need to move the charging station between classrooms. When deciding on a location, consider its proximity to a power source such as a power strip or wall outlet.