The slots in the TI Charging Station CE are designed to accommodate a graphing calculator without a slide case attached. The calculator will not fit in the slots with the slide case attached.
The front of the calculator must face the front of the charging station. You may damage the TI-84 Plus CE Python graphing calculator if you try to force it into the charging station facing the wrong direction. When looking at the TI logo on the charging station, insert calculators into the slot with the keypad facing left.
1. | Remove the slide case from the graphing calculator. |
2. | Align the grooves on the sides of the graphing calculator with the guides in the charging station slots. Ensure the calculator is facing the proper direction. |
3. | Gently push the graphing calculator into the slot. You will feel a slight resistance; continue pushing down until the graphing calculator is seated. |
If your calculator has an LED light on the side, the calculator is properly seated when the LED turns amber to indicate charging.