Menus and Functions

• To quit the App, select the QUIT-APP option at the upper-right of the Y=screen. Select 2:Quit Transfrm at the prompt.
• Inequality Graphing App and Transformation Graphing App cannot run at the same time since they enhance the Function Mode of the o editor. If the Apps are in conflict, follow the prompts to quit the conflicting App, which will allow the other App to run as an enhanced o editor.
• The Transformation Graphing App is best used for animation graphing investigations. The window variable Xres is set to 3 when the app launches. This plots every third graphing pixel and provides the best experience when using animations for Y1 and/or Y2. While Xres can be set to 1 in p, your general graphing experience without animations will be optimal in the standard graphing mode where Xres defaults to 1.

Menus

Description

Graph/Plot Setup Keys

o

Displays the o Editor, where you can:

• enter one or more functions
• animate functions in Y1 and/or Y2
• graph functions using Y3-Y0
• graph up to three plots
• change the graph color
• change the transformation play type
• select a function format to paste for Y1 and/or Y2
• change the color and line style of Y3-Y0

 

Press | until the cursor is over the style column at the left of the Yn function. Press [enter]. Navigate to the options using †. Press | or ~ on a spinner menu to make a selection. Select OK or CLEAR to accept or dismiss the changes.

Play-Pause (3)

Controls which coefficient is changed and when the graph is plotted.

Play
(1)

Stores a series of changes as pictures to display in a slide show format. The pictures play in a continuous loop until you stop them. Use [enter] and then É to stop animations.

*See Note following the table.

Play Fast
(2)

Stores a series of changes as pictures to display in a slide show format. The pictures play in a continuous loop until you stop them. It displays the pictures at a more rapid rate than Play. Use [enter] and then É to stop animations.

*See Note following the table.

p

Set the viewing window to produce the best display of your graph.

q

Quickly adjust the window to a pre-defined setting.

r

Move the cursor along the graphed function using | and ~.

s

Display the graph you have defined.

[SETUP]

On the graph screen, pressing [SETUP] (s) will display the SETTINGS menu where you can select animation play types, TrailOff/TrailOn setting, and set the values of the parameters A, B, C, or D (if entered in Y1 and/or Y2). Press s on the SETTINGS screen to display the graph.

TrailOff
TrailOn

In y ., TrailOn leaves a dotted graph style of each graph as the coefficient is changed or animated. Default is TrailOff.

*Note: A memory error occurs if there are more than 13 screens to create for the animation. Press p and } to SETTINGS. Change the parameter start value, the step and/or the Max so the sequence of screens requested remains at most 13.

More Information

See the graphing calculator’s Reference Guide for information on system error messages.

See the original app guidebook for more details on this application. Visit education.ti.com/go/download.