Menus and Functions

Each simulation has features appropriate for the type of simulation. The table below is a quick guide to see the features and options in each simulation.

• The main menu will appear when you open the App.
• Press ESC (press o) and YES (press o) to return to the main menu from a simulation.
• To exit the application, select QUIT (press s) from the main menu.

Menus

Functions

Main Menu

Toss Coins

Creates a simulation of a two-sided coin toss, and you have the option to weight the sides of the coin. You can flip up to 3 coins at once, and the number of heads is tallied.

Roll Dice

Creates a simulation of rolling up to three dice. The type of dice includes 6, 8, 10, 12, and 20 sides. The sum of the faces is tallied.

Pick Marbles

Creates a simulation of picking up to 5 different marbles from a bag. The simulation can run with or without replacement. The number of each type of marble in each pick is tallied.

Spin Spinners

Creates a simulation of one spinner with between 2 and 8 sections. Each section can be weighted. The spinner results are tallied.

Draw Cards

Creates a simulation of drawing one card at a time from a 52- or 32-card deck. For each pick, the number and suit are tallied. The draw of a card from the deck can be set with or without replacement from each draw. You can only use one deck at a time.

Random Numbers

Generates (draws) a set of up to 6 random numbers. The number range can be set from 0 to 99. Repetition or no repetition of numbers from the range can be set as an option. Each draw of the random set is tallied on the screen.

OK

Open the selected simulation.

SEED

Set the random seed value.

ABOUT

App version number information.

QUIT

Exit the application.

Toss Coins

ESC

Return to the previous screen

TOSS

Toss one coin and access more tosses.

SET (Settings)

Change the settings for the simulation.

Trial Set

Tosses coin(s) as per trial settings and allows shortcut option to toss +1, +10, or +50 more tosses to add on to the simulation. Enter trial value from 1 to 999 tosses.

Coins

Set the number of coins tossed per trial to 1, 2, or 3.

Graph

Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values.

StoTbl (Store Table)

Set to No, All, or 50 to control the trials displayed in the table view.

ClearTbl (Clear Table)

Set to Yes if you want to clear the data of an existing simulation.

Updates (Update After)

Number of trials before the graph and data are updated.

DATA

Save the collected data to a list.

TABLE

Show a table of the trials.

GRAPH

Show a graph of the trials.

Roll Dice

ESC

Return to the previous screen

ROLL

Rolls a die or dice as per trial settings and allows shortcut option to toss +1, +10, or +50 more rolls to add on to the simulation.

SET (Settings)

Change the settings for the simulation.

Trial Set

Enter trial value from 1 to 999.

Dice

Set the number of die or dice tossed per trial to 1, 2, or 3.

Sides

Set number of sides to 6, 8, 10, 12, or 20.

Graph

Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values.

StoTbl (Store Table)

Set to No, All, or 50 to control the trials displayed in the table view.

ClearTbl (Clear Table)

Set to Yes if you want to clear the data of an existing simulation.

Updates (Update After)

Number of trials before the graph and data are updated.

DATA

Save the collected data to a list.

TABLE

Show a table of the trials.

GRAPH

Show a graph of the trials.

Pick Marbles

ESC

Return to the previous screen

PICK

Pick number of marbles as per trial settings.

SET (Settings)

Change the settings for the simulation.

Trial Set

Enter trial value from 1 to 999.

Types

Set the number of different types of marbles in the simulation to 1, 2, or 3.

Graph

Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values.

StoTbl (Store Table)

Set to No, All, or 50 to control the trials displayed in the table view.

ClearTbl (Clear Table)

Set to Yes if you want to clear the data of an existing simulation.

Replace

Yes: Replaces the marble after it is drawn. No: The marble is removed when it is drawn.

Updates (Update After)

Number of trials before the graph and data are updated.

DATA

Save the collected data to a calculator list.

TABLE

Show a table of the trials.

GRAPH

Show a graph of the trials.

Spin Spinner

ESC

Return to the previous screen.

SPIN

Spins the spinner as per trial settings and allows shortcut option to toss +1, + 10, or +50 more spins to add on to the simulation.

SET (Settings)

Change the settings for the simulation.

Trial Set

Enter trial value from 1 to 999.

Sections

Set the number of sections of the spinner from 2 to 8 sections.

Graph

Set graph display to frequency or simulated probability. Use right and left arrows on the bar graph view to display these values.

StoTbl (Store Table)

Set to No, All, or 50 to control the trials displayed in the table view.

ClearTbl (Clear Table)

Set to Yes if you want to clear the data.

Updates (Update After)

Number of trials before the graph and data are updated.

DATA

Save the collected data to a list.

TABLE

Show a table of the trials.

GRAPH

Show a graph of the trials.

Draw Cards

ESC

Return to the previous screen

DRAW

Draw one card.

SET (Settings)

Change the settings for the simulation.

Decks

Set to 1, 2, or 3 decks.

Replace

Yes: Replaces the card after it is drawn.

No: The card is removed when it is drawn.

Deck Size

Set the card deck size to 52 or 32 cards.

DATA

Save the collected data to a list.

CLEAR

Clear all trials from memory.

Random Number Sets

ESC

Return to the previous screen.

Draw

Roll one dice.

SET (Settings)

Change the settings for the simulation.

Numbers

Set between 1 and 6 random numbers per draw.

Range

Enter the range of numbers from 0 to 99.

Repete

Yes: Reuse numbers after they have been chosen.

No: each trial will be unique.

DATA

Save the collected data to a list.

CLEAR

Clear all trials from memory.

Advanced Options Menu

ADV (Advanced)

Set weight or probabilities for Toss Coin, Roll Dice, or Spin Spinner outcomes. Set the amount of each different marble in the simulation for Pick Marbles.

More Information

See the graphing calculator’s Reference Guide for information on system error messages.

See the original app guidebook for more details on this application. Visit education.ti.com/go/download.