Menus and Functions

• To quit the App, select the QUIT-APP option at the upper-right of the Y=screen. Select 2:Quit Inequal at the prompt.
• Inequality Graphing App and Transformation Graphing App cannot run at the same time since they enhance the Function Mode of the o editor. If the Apps are in conflict, follow the prompts to quit the conflicting App, which will allow the other App to run as an enhanced o editor.

Menus

Functions

Graph/Plot Setup Keys

Y=

Displays the Y= Editor, where you can enter one or more inequalities to graph and change the graph color and line style.

X=

Graph a vertical inequality.

Window

Set the viewing window to produce the best display of your graph.

Zoom

Quickly adjust the window to a pre-defined setting.

Trace

Move the cursor along the graphed function using | and ~.

Graph

Display the graph you have defined..

Inequality Menu

INEQUALITY

 

1: Point of Interest Trace

Trace points of interest (such as intersections) b.etween relations.

2: Inequal Intersection

Display the intersection of the inequalities and select the color of the shading.

3: Union

Display the combined area of the inequalities and select the color of the shading.

4: Original ShadeRes=

Return to the original inequality graph.

5: Inequality App Help

Help for Inequality Graphing.

Quit Menu

1: Continue Running

Continue using the Inequality Graphing app.

2: Quit

Quit the App.

3: About

Display the opening screen with version number information.