Menus and Functions

To quit the App, press [Quit] (s).

Menus

Functions

Main Menu

File

Save the data from an experiment or select New and Vernier EasyData™ App restarts in the default data-collection mode, and the default settings are restored.

Setup

Set up the experiment.

The menu will differ depending on the sensor. For example, for connected CBR 2™ motion detector, the setup menu displays as follows:

Time Graph

Open the Time Graph Settings wizard.

Sample Interval

Set the interval in seconds. Select Next to go to the next setting.

Number of Samples

Set the total number of samples to collect.

Experiment Length

Set the length of the experiment in seconds.

Edit

Edit the time graph settings.

Cancl

Cancel your changes and return to the previous settings.

OK

Return to the main menu.

Events with Entry

Capture samples manually for a set of events that you define. Each sampled value becomes a y-value; you enter the x-value.

Keep

Capture the current sampled (y) value.

Enter value

Assign an x-value to define the data point. Then select OK.

Stop

Select Stop to end the experiment. The data points are displayed as a graph (a calculator scatter plot).

Main

Return to the main menu.

Zero

Use the current data reading as a zero reference.

Start

Start collecting data.

Stop

Stop collecting data. A scaled graph of the collected data appears.

Main

Return to the main menu.

Graph

Graph the resulting equation.

Adv

Select independent and dependent lists to plot various views of the data.

Plots

Plot options such as distance vs. time, velocity vs. time, and acceleration vs. time (dependent on sensor connected).

Anlyz

Computes statistics on data collected and finds a variety of regression fit to data (dependent on sensor connected).

Scale

Options to auto-fit or manually edit the graph scaling.

Quit

Quit the application. The collected data has been transferred to the calculator’s lists.