Example Activity - Vernier EasyData™

Use this activity to learn the basics of the App.

1. Connect the Vernier EasyTemp™ sensor to the calculator. After a few seconds, the Vernier EasyData™ main screen displays. This main screen shows the current Vernier EasyData™ mode and the current sensor reading in a meter format.
2. Select Start to start collecting data, and then wait five seconds.

3. Hold the tip of the Vernier EasyTemp™ sensor for about 30 seconds. The graph shows the temperature as it changes.

 

4. Select Stop to stop collecting data. Vernier EasyData™ displays a scaled graph of the sampled temperatures.

5. Press ~ repeatedly to scroll the cursor to the right, and note the temperature at each data point.
6. When you finish exploring the graph, select Main to return to the Vernier EasyData™ main screen.

 

Tip: On the graph screen, select [Anlyz] (q) to see all the features to analyze the data.

Tip: On the main screen with the sensor reading in meter format, press [Setup] (p) to choose activities designed for the connected sensor.

 

7. Select Quit. A message indicates that Vernier EasyData™ has stored the collected data in calculator lists.