Menus and Functions

• To display the CELLSHEET MENU, select Menu (press b).
• To display a help screen for common tasks, select Help from the CELLSHEET MENU.
• To exit the application, select Quit CellSheet from the CELLSHEET MENU.
• Press ‘ or y 5 to:
- Return to the main menu from a submenu.
- Return to the spreadsheet from the main menu.

Menus

Functions

File Menu

1: Open...

Opens an existing spreadsheet file.

2: Save As...

Saves the current spreadsheet with the same name or with a different name.

3: New...

Creates a new spreadsheet and allows you to use a new or existing name.

4: Delete...

Deletes a spreadsheet. You cannot delete the currently open spreadsheet.

5: Format...

Sets up formatting options.

(Default values are highlighted.)

AutoCalc: Y N

Cursor Mvmt: † ~

Init Help: Y N

Show: FMLA VALUE

6: Recalc

Recalculates the spreadsheet (only needed when the autocalculation feature in the FORMAT menu is turned off).

Edit Menu

1: Go To Cell...

Moves the cursor to a specific cell.

2: Undelete Cell

Retrieves the contents of the cell that you just deleted or cleared.

3: Clear Sheet...

Deletes all data from the current spreadsheet.

4: Select Range...

Selects a range of cells.

5: Cut

Cuts the contents and formulas from the currently selected cell, or range of cells, and places them on the clipboard.

Shortcut key: _

6: Copy

Copies the contents and formulas from the currently selected cell, or range of cells, and places them on the clipboard.

Shortcut key: `

7: Paste

Pastes the contents and formulas that were just cut or copied to the clipboard into the current cell.

Shortcut key: a

Options Menu

1: Statistics...

Calculates linear regression for the currently selected cell range.
1: 1-variable statistics
2: 2-variable statistics

3: Linear Regression - LinReg(ax+b)

2: Fill Range...

Fills a range of cells with a formula, number, or text.

 

3: Sequence...

Fills a range of cells with a sequence of numbers.

1st Cell:

seq(

DownRight

4: Import/Export ...

Imports and exports calculator files such as lists, matrices, or variables.

5: Sort...

Sorts a range of cells in ascending or descending order.

6: Col Decimal...

Sets the decimal mode display for a column. The calculator decimal mode display (accessed by pressing z) does not affect the CellSheet™ application.

Charts Menu

1: Scatter...

Displays a scatter chart for a range of cells.

XRange:

YRange 1:

YRange 2:

YRange 3:

Title:

AxesOn AxesOff

DrawFit Draw

Notes:

• You can set the color of the graph using the color spinner in the left column. After you enter a range, move the cursor to the color spinner and press [enter]. Next, use | ~ to select a new color. Press † to set the new color.
• DrawFit Autoscales the graph of the chart. Draw uses the chart window settings in the CellSheet Chart menu (not the Operating System Window settings) to graph the chart.

2: Scatter Window

Displays the parameters for the viewing window for the scatter chart so that you can change the values.

Xmin=

Xmax=

Xscl=

Ymin=

Ymax=

Yscl=

Draw Save

3: Line...

Displays a line chart for a range of cells.

XRange:

YRange 1:

YRange 2 :

YRange 3:

Title:

AxesOn AxesOff

DrawFit Draw

Notes:

• You can set the color of the graph using the color spinner in the left column. After you enter a range, move the cursor to the color spinner and press [enter]. Next, use | ~ to select a new color. Press † to set the new color.
• DrawFit Autoscales the graph of the chart. Draw uses the chart window settings in the CellSheet Chart menu (not the Operating System Window settings) to graph the chart.

4: Line Window...

Displays the parameters for the viewing window for the line chart so that you can change the values.

Xmin=

Xmax=

Xscl=

Ymin=

Ymax=

Yscl=

Draw Save

5: Bar...

Displays a bar chart for a range of cells.

Categories:

Series1:

Ser1Name:

Series2:

Ser2Name:

Series3:

Ser3Name:

Title:

Vertical Horiz

DrawFit Draw

Notes:

• You can set the color of the graph using the color spinner in the left column. After you enter a range, move the cursor to the color spinner and press [enter]. Next, use | ~ to select a new color. Press † to set the new color.
• Vertical Horiz display the bars in specified directions.
• DrawFit Autoscales the graph of the chart. Draw uses the chart window settings in the CellSheet Chart menu (not the Operating System Window settings) to graph the chart.

6: Bar Window

Displays the parameters for the viewing window for the bar chart so that you can change the values.

Barmin=

Barmax=

Draw Save

7: Pie...

Displays a pie chart for a range of cells.

Categoreis:

Series:

Number Percent

Title:

Draw: