Browsing the TI-84 Plus CE Catalog

Selecting an Item from the CATALOG

To browse and select a CATALOG item, follow these steps.

1. Press y Nto display the CATALOG.

The 4 in the first column is the selection cursor.

2. Press † or } to scroll the CATALOG until the selection cursor points to the item you want.
• To jump to the first item beginning with a particular letter, press that letter; alpha-lock is on.
• Items that begin with a number are in alphabetical order according to the first letter after the number. For example, 2‑PropZTest( is among the items that begin with the letter P.
• Functions that appear as symbols, such as +, L1, <, and $(, follow the last item that begins with Z. To jump to the first symbol, !, press [q].
3. Press Í to paste the item to the current screen.

Note:

• From the top of the CATALOG menu, press } to move to the bottom. From the bottom, press † to move to the top.
• When your TI‑84 Plus CE is in MathPrint™ mode, many functions will paste the MathPrint™ template on the home screen. For example, abs( pastes the absolute value template on the home screen instead of abs(.


MathPrint™


Classic