|
|
---|---|
Param Sets parametric graphing mode. |
† z |
|
|
---|---|
Pause Suspends program execution until you press Í. |
† ¼ |
Pause |
|
---|---|
Pause [value] Displays value; suspends program execution until you press Í. |
† ¼ |
|
|
---|---|
Pause [value, time] Displays value on the current home screen and execution of the program continues after the time period specified. For time only, use Pause “”,time where the value is a blank string. Time is in seconds. Pause value,time. |
† ¼ |
|
|
---|---|
piecewise( New piecewise function to support entry of functions as they are seen in textbook. This command can be found in » MATH B:piecewise( |
» } or † to scroll to B:piecewise( |
|
|
---|---|
Plot#(type,Xlist,Ylist[,mark,color#]) Defines Plot# (1, 2, or 3) of type Scatter or xyLine for Xlist and Ylist using mark and color. Color#: 10 - 24 or color name pasted from [vars] COLOR. Note: Xlist and Ylist represent the Xlist and Ylist names. |
† y , |
Plot1( Plot2( Plot3( |
|
---|---|
Plot#(type,Xlist,[,freqlist,color#]) Defines Plot# (1, 2, or 3) of type Histogram or Boxplot for Xlist with frequency freqlist and color #. Color#: 10 - 24 or color name pasted from [vars] COLOR. Note: Xlist represents the Xlist name. |
† y , |
Plot1( Plot2( Plot3( |
|
---|---|
Plot#(type,Xlist,[,freqlist,mark,color#]) Defines Plot# (1, 2, or 3) of type ModBoxplot for Xlist with frequency freqlist using mark and color #. Color#: 10 - 24 or color name pasted from [vars] COLOR. Note: Xlist represents the Xlist name. |
† y , |
Plot1( Plot2( Plot3( |
|
---|---|
Plot#(type,datalist,[,data axis,mark,color#]) Defines Plot# (1, 2, or 3) of type NormProbPlot for datalist on data axis using mark and color # data axis can be X or Y. Color#: 10 - 24 or color name pasted from [vars] COLOR. Note: datalist represents the datalist name. |
† y , |
|
|
---|---|
PlotsOff [1,2,3] Deselects all stat plots or one or more specified stat plots (1, 2, or 3). |
y , |
|
|
---|---|
PlotsOn [1,2,3] Selects all stat plots or one or more specified stat plots (1, 2, or 3). |
y , |
|
|
---|---|
Pmt_Bgn Specifies an annuity due, where payments occur at the beginning of each payment period. |
Œ 1:Finance |
|
|
---|---|
Pmt_End Specifies an ordinary annuity, where payments occur at the end of each payment period. |
Œ 1:Finance |
|
|
---|---|
poissoncdf(m,x) Computes a cumulative probability at x for the discrete Poisson distribution with specified mean m. |
y = |
|
|
---|---|
poissonpdf(m,x) Computes a probability at x for the discrete Poisson distribution with the specified mean m. |
y = |
|
|
---|---|
Polar Sets polar graphing mode. |
† z |
4Polar |
|
---|---|
complex value 4Polar Displays complex value in polar format. |
» |
|
|
---|---|
PolarGC Sets polar graphing coordinates format. |
† y . |
|
|
---|---|
Executes the program name. |
† ¼ |
|
|
---|---|
GPrn(pmt1,pmt2[,roundvalue]) Computes the sum, rounded to roundvalue, of the principal amount between pmt1 and pmt2 for an amortization schedule. |
Œ 1:Finance |
|
|
---|---|
prod(list[,start,end]) Returns product of list elements between start and end |
y 9 |
|
|
---|---|
Prompt variableA[,variableB,...,variable n] Prompts for value for variableA, then variableB, and so on. |
† ¼ |
|
|
---|---|
1‑PropZInt(x,n[,confidence level]) Computes a one-proportion z confidence interval. |
† … |
|
|
---|---|
2‑PropZInt(x1,n1,x2,n2[,confidence level]) Computes a two-proportion z confidence interval. |
† … |
|
|
---|---|
1‑PropZTest(p0,x,n[,alternative,drawflag, color#]) Computes a one-proportion z test. alternative=L1 is <; alternative=0 is ; alternative=1 is >. drawflag=1 draws results; drawflag=0 calculates results. Color#: 10 - 24 or color name pasted from [vars] COLOR. |
† … |
|
|
---|---|
2‑PropZTest(x1,n1,x2,n2[,alternative,drawflag, color#]) Computes a two-proportion z test. alternative=L1 is <; alternative=0 is ; alternative=1 is >. drawflag=1 draws results; drawflag=0 calculates results. Color#: 10 - 24 or color name pasted from [vars] COLOR. |
† … |
|
|
---|---|
Pt‑Change(x,y[,color#]) Toggles a point on or off at (x,y) on the graph area. Off will be in the Background color and On will be the specified Color#: 10 - 24 or color name pasted from [vars] COLOR. |
y < |
|
|
---|---|
Erases a point at (x,y) on the graph area using mark. The Off state may be the background color determined by the ImageVar or color setting. Color#: 10 - 24 or color name pasted from [vars] COLOR. |
y < |
|
|
---|---|
Pt‑On(x,y[,mark,color#]) Draws a point at (x,y) on the graph area using mark and the specified color#. Color#: 10 - 24 or color name pasted from [vars] COLOR. |
y < |
|
|
---|---|
PwrReg [Xlistname,Ylistname,freqlist,regequ] Fits a power regression model to Xlistname and Ylistname with frequency freqlist, and stores the regression equation to regequ. |
… |
|
|
---|---|
Pxl‑Change(row,column[,color#]) Toggles Off to On in the graph area: with specified color# Color#: 10 - 24 or color name pasted from [vars] COLOR. |
y < |
|
|
---|---|
Pxl‑Off(row,column) The Off state will display the set Background Image Var or COLOR. |
y < |
|
|
---|---|
Pxl‑On(row,column[,color#]) Draws pixel on the graph area at (row,column) in the specified color. Color#: 10 - 24 or color name pasted from [vars] COLOR. |
y < |
|
|
---|---|
pxl‑Test(row,column) Returns 1 if pixel (row, column) is on, 0 if it is off; |
y < |
|
|
---|---|
P4Rx(r,q) Returns X, given polar coordinates r and q or a list of polar coordinates. |
y ; |
P4Ry( |
|
---|---|
P4Ry(r,q) Returns Y, given polar coordinates r and q or a list of polar coordinates. |
y ; |