Copying and Renaming a Program

To copy all command lines from one program into a new program, follow steps 1 through 4 for Creating a New Program, and then follow these steps.

1. Press y K. Rcl is displayed on the bottom line of the program editor in the new program.
2. Press ¼ to display the PRGM EXEC menu.
3. Select a name from the menu. prgmname is pasted to the bottom line of the program editor.
4. Press Í. All command lines from the selected program are copied into the new program.

Copying programs has at least two convenient applications.

• You can create a template for groups of instructions that you use frequently.
• You can rename a program by copying its contents into a new program.

Note: You also can copy all the command lines from one existing program to another existing program using RCL.