Sending a TI-Basic Program to a Calculator

You can send a program to a connected calculator.

To send a program to a connected calculator

1. If you have not already done so, save the program.
2. Click .
FILE NAME: This may differ from the NAME ON CALCULATOR depending on what you named the program on your computer.
NAME ON CALCULATOR: select the program name (it should be the default, but you may change the program name by clicking Custom).

LOCATION: Choose whether you save the program in the calculator's RAM or Archive.
DESTINATION CALCULATORS: Select whether you want to send the program to all connected calculators, or just selected calculators (from a check list).

To send programs to multiple calculators

1. Select the Select Calculators button on the dialog box.
2. Check the boxes to next to the calculators you want to select.
3. Click Send.

Language Settings

If you wish to develop a TI-Basic program in a language different than your computer OS language setting, you can re-launch TI Connect™ CE in another language.

1. Select File > Change Language.
2. Select the language change after restart of the application.

QUIT LATER - Retains the language selected and TI Connect™ CE will launch in this selected language the next time TI Connect™ CE is launched.
QUIT NOW - Closes the software app. TI Connect™ CE will launch in this selected language the next time TI Connect™ CE is launched.
CANCEL - No language change. Computer OS language will be the default.