This Screen Capture only feature provides a way to take a screen capture of a graph on the high resolution calculators, crop to the graph area and then convert only the graph area to a Background Image. Check Graph Area Only to create this type of Background Image.
1.
If you have not already done so, capture the screen.
2.
Click the screen capture to select it.
3.
Click
•
FILE NAME: This may differ from the NAME ON CALCULATOR depending on what you named the screen capture on your computer.
•
NAME ON CALCULATOR: select the background image (it should be the default, but you may change the background image name using this menu).
Note: Screen captures and converted image files will be sent as Pic Vars to gray scale calculators.
•
GRAPH AREA ONLY: In the right panel, select whether you want to send just the graph area, or the entire screen. When sending a screen capture back to a calculator, it is best to send the graph area only.
Cropping an Image
A screen capture of the graph area includes the full screen of the TI‑84 Plus CE, status bar, graph border, and the graph area.
TI Connect™ CE software allows you to crop the image to a Graph Area Only size to create a Background Image Var. You can crop a screen to Graph Area only in the Send to in the Send to Calculators dialog box.
•
DESTINATION CALCULATORS: Select whether you want to send the image to all connected calculators, or just selected calculators (from a check list).
To send files to multiple calculators
1.
Select the Select Calculators button on the dialog box.
2.
Check the boxes to next to the calculators you want to select.