|
|
– | Create ti_hub/ti_rover Python programs in the CE emulator running the Python App. |
*Note: There is no connectivity between TI-SmartView™ CE and TI-Innovator™ Hub or TI-Innovator™ Rover. Programs can be created and then run on the CE calculator.
– | Quit the Python App to prepare to transfer the Python AppVar(s) from the emulator. The emulator should not “be busy” running an App or program for the next step. |
– | Change to the Emulator Explorer workspace and send the program(s) to the computer. |
– | Use TI Connect™ CE to send the Python AppVars from the computer to the CE calculator for the TI-Innovator™ Hub/TI-Innovator™ Rover experience. |
Note: To break a running Python program in the Shell, such as if a program is in a continuous loop, press [on]. Press [Tools] [zoom] > 6:New Shell as an alternate method to halt a running program.
Reminder: For any computer/TI-Python experience: After creating a Python program in a Python development environment on the computer, please validate your program runs on the calculator/emulator in the TI-Python experience. Modify the program as needed.
– | When running the SmartPad CE App on your connected CE will behave as a remote keypad including the special keypad mapping offered when the Python App is running. |
– | Please quit the Python App so the emulator is not busy when you access the full features of the Emulator Explorer workspace. |
– | program.py < > PY AppVar conversions are allowed. This is similar to the TI Connect™ CE experience when sending programs to the connected CE calculator. |
– | When sending a program.py file created in another Python environment, your PY AppVar will need to be edited to run as expected in TI-Python. Use the Python App Editor to modify as needed for the unique modules such as ti_plotlib, ti_system, ti_hub and ti_rover. |
– | *.csv files of data, formatted as stated in the wizard dialog, will convert data into CE list variables. Methods in ti_system can then be used to share lists between the emulator CE OS and the Python App. This feature is similar to the Data Import Wizard in TI Connect™ CE. |
- | If decimal numbers are represented with the use of a comma in the *.csv file, the file will not convert using the Data Import Wizard. Please check your computer operating system number formatting and convert the *.csv to use the decimal point representation. The calculator list and matrix editor use the number format as, for example, 12.34 and not 12,34. |