Using Menus

When you press a key or key combination to display a menu, one or more menu names appear on the top line of the screen.

The menu name on the left side of the top line is highlighted. Up to nine items in that menu are displayed, beginning with item 1.
A number or letter identifies each item’s place in the menu. The order is 1 through 9, then 0, then A, B, C. Once number and letter options are exhausted, the item number or letter area will be blank. Select these items using the arrow keys.
When the menu continues beyond the displayed items, a down arrow ($) replaces the colon next to the last displayed item.
When a menu item ends in an ellipsis (...), the item displays a secondary menu, editor, or wizard when you select it.
Use Catalog Help for more syntax help when needed. Select a menu item and then press à to go to a syntax help editor (if the menu item is supported).