Error Message |
Description |
||||||
---|---|---|---|---|---|---|---|
Not Enough Memory! Add. RAM needed. |
Cabri™ Jr. needs at least 4802 free bytes to run (roughly 5k). The dialog box indicates how much more free memory you need to be able to run Cabri™ Jr. It is possible to make more RAM or Flash memory available to Cabri™ Jr., by removing files stored in RAM or in Flash. Refer to the calculator manual for more information. |
||||||
Continue without Undos? |
When more than 128 objects have been drawn, Undo must be disabled to continue. After this error message is displayed, a dialog box asks if you want to continue. If you continue, Undo is disabled Undo will be automatically re-enabled if the number of objects becomes lower than 128. |
||||||
Max. object# reached. |
Cabri™ Jr. figures can have a maximum of 256 objects. |
||||||
Not Enough Memory! to save file.
|
When this message displays, the current figure is not lost. You can save the figure by:
|
||||||
No figure to open! |
You have selected Open from the F1 menu, but there are no saved figures on your calculator to open. |
||||||
Name already exists! Continue anyway? |
You have entered a file name for your figure that already exists. Select OK to overwrite the existing file, or select No to return to the Save dialog box so that you can enter a different file name. |
||||||
CURRCAJU is reserved |
You cannot use or CURRCAJU or CURRCAJ2 as a file name. They are reserved AppVar names. |
||||||
Figure abc not re-archived!
|
This happens, under tight Flash RAM conditions, when you have worked with an archived figure and made it significantly larger. In this case, you may not have enough memory to save the figure in Flash RAM, so the App saves it as a regular AppVar in RAM.
|
||||||
Batteries too low to access archived files! |
The batteries in your calculator are low, so the App cannot save the file into Flash RAM . You can save the file without archiving it, then change the batteries and archive the file later. |
See the graphing calculator’s Reference Guide for information on system error messages.
See the original app guidebook for more details on this application. Visit education.ti.com/go/download.