You are here: Reference Guide for the TI-84 Plus CE Graphing Calculator > CATALOG, Strings, Hyperbolic Functions > Selecting an Item from the CATALOG

Browsing the TI-84 Plus CE Catalog

Selecting an Item from the CATALOG

To browse and select a CATALOG item, follow these steps.

1. Press y Nto display the CATALOG.

The 4 in the first column is the selection cursor.

2. Press or } to scroll the CATALOG until the selection cursor points to the item you want.
To jump to the first item beginning with a particular letter, press that letter; alpha-lock is on.
Items that begin with a number are in alphabetical order according to the first letter after the number. For example, 2‑PropZTest( is among the items that begin with the letter P.
Functions that appear as symbols, such as +, L1, <, and $(, follow the last item that begins with Z. To jump to the first symbol, !, press [q].
3. Press Í to paste the item to the current screen.

Note:

From the top of the CATALOG menu, press } to move to the bottom. From the bottom, press to move to the top.
When your TI‑84 Plus CE is in MathPrint™ mode, many functions will paste the MathPrint™ template on the home screen. For example, abs( pastes the absolute value template on the home screen instead of abs(.


MathPrint™


Classic