You are here: TI-Basic Programming Guide for the TI CE Family of Graphing Calculators > Entering Command Lines and Executing Programs > Entering a Program Command Line

Entering a Program Command Line

You can enter on a command line any command, instruction, or expression that you could execute from the home screen. In the program editor, each new command line begins with a colon. To enter more than one instruction or expression on a single command line, separate each with a colon.

Note: A command line can be longer than the screen is wide.

While in the program editor, you can display and select from menus. You can return to the program editor from a menu in either of two ways.

• Select a menu item, which pastes the item to the current command line.

— or —

• Press u.

When you complete a command line, press Í. The cursor moves to the next command line.

Programs can access variables, lists, matrices, and strings saved in memory. If a program stores a new value to a variable, list, matrix, or string, the program changes the value in memory during execution.

You can call another program as a subroutine.