You are here: TI-Basic Programming Guide for the TI CE Family of Graphing Calculators > Editing a Program

Editing Programs

In this section you will follow steps to edit a program. This section describes how to insert and delete command line.

Editing a Program

To edit a stored program, follow these steps.

1. Press ¼ ~ to display the PRGM EDIT menu.
2. Select a program name from the PRGM EDIT menu. Up to the first nine lines of the program are displayed.

Note: The program editor does not display a $ to indicate that a program continues beyond the screen.

3. Edit the program command lines.
• Move the cursor to the appropriate location, and then delete, overwrite, or insert.
• Press u to clear all program commands on the command line (the leading colon remains), and then enter a new program command.

Note: To move the cursor to the beginning of a command line, press y |; to move to the end, press y ~. To scroll the cursor down seven command lines, press t †. To scroll the cursor up seven command lines, press t }.

Inserting and Deleting Command Lines

To insert a new command line anywhere in the program, place the cursor where you want the new line, press y 6, and then press Í. A colon indicates a new line.

To delete a command line, place the cursor on the line, press u to clear all instructions and expressions on the line, and then press { to delete the command line, including the colon.